DUG_LK FUGA - Wiser wireless socket outlet 1½ M_WH-00

Anti-Tripping Management

The Anti-Tripping Management prevents the circuit breaker from tripping by switching off the load (e.g. Water Heater, EV Socket) or reducing the power of the load.

The Power Consumption Management (PCM) system is an advanced algorithm designed to prevent global overconsumption. It achieves this by reducing setpoints and shutting down specific loads, ensuring that overall energy consumption stays within a predefined limit. With the integration of Wiser Home, users gain enhanced control over the loads monitored by the PCM. You can enroll up to eight loads at a time, which helps maintain the total consumption of the system below the established limit. This limit is determined by your contract specifications, so it's important to refer to the Setting Tariff section for information on peak and off-peak rates. Eligible devices will be automatically incorporated into the Anti-Tripping Management system, further optimizing energy usage and enhancing the overall efficiency of your home energy management.

For more information on Anti-Tripping Management refer to the respective System User Guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.