DUG_LK FUGA - Wiser wireless socket outlet 1½ M_WH-00

Setting the LED indicator behaviour

Using the Wiser Home app, you can set the state of LED indicator when the socket is turned ON.
By default, the LED turns ON, when the socket is turned ON.
  1. On the Home page, tap .
  2. Tap Devices > Connected Socket > LED Indicator Behaviour (A) and select one of the following options as per your preference:

    LED On when Power is On

    The LED turns ON when the device is ON.

    LED Off when Power is On

    The LED turns OFF when the device is ON.

    Always Off

    The LED stays OFF all the time.

    Always On

    The LED stays ON all the time.

  3. Tap Done.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.