DUG_LK FUGA - Wiser wireless socket outlet 1½ M_WH-00

Monitoring energy consumption

Using the Wiser app, you can monitor the energy consumption of the load connected to the device.
  1. On the Control tab, tap All > Connected Socket.
  2. When the socket outlet is turned on, the power consumption is displayed in watts (W).
    TIP: The power consumption varies depending on the load connected to the socket outlet.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.