DUG_LK FUGA - Wiser wireless socket outlet 1½ M_WH-00

About the device

The LK FUGA ® Wiser wireless socket outlet 1½ M (hereinafter referred to as Socket Outlet) is a connected electrical outlet designed to manage and control electrical devices in a convenient and efficient manner. You can remotely control and monitor the energy consumption of the plugged-in load. The Socket outlet is equipped with a temperature and overload protection and mechanism. When the Socket outlet is used with a high load, the mechanism can switch off the Socket outlet, help to ensure overheat and overload protection.

NOTE:
  • Do not connect any devices that depend on a permanent power supply.

  • Do not mix different load types in the controlled socket.

  • Do not use multi-sockets in the controlled socket.

  • Do not use for EV charging.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.