DUG_Odace Multiwire Rotary Dimmer_WH-01

Operating a Dimmer

You can switch the dimmer ON/OFF and adjust its brightness using the paired Wireless switch.
  • Short press the top (ʌ+) or bottom (v-) of the Wireless switch (< 0,5 s) to turn ON/OFF the connected load (A).

  • Long press the top (ʌ+) or bottom (v-) of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?