DUG_Odace Multiwire Rotary Dimmer_WH-02

Pairing Wireless Switch with Rotary Dimmer

  1. Remove the rocker from the Wireless switch and short press the upper push button (A) 5 times in quick succession.
    The status LED blinks green.
  2. Remove the knob from the Rotary Dimmer and short press the push button 5 times in quick succession.
    The status LED blinks green.

    The light connected to the Rotary Dimmer blinks for a few times. The status LED stops blinking green on the Wireless switch and the Rotary Dimmer. The Rotary Dimmer can now be controlled by the Wireless switch.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.