DUG_Odace Multiwire Rotary Dimmer_WH-01

Resetting the device

You can reset the dimmer to factory default manually.
  • Remove the knob and short-press the push button 3 times (<0.5 s) and then long-press the push button once (>10 s).

  • After 10 s, the LED starts blinking red and then release the push button.

  • Upon successful reset, the LED stops blinking.

  • The dimmer restarts and blinks green for a few seconds.

NOTE: After reset, the LED turns amber indicating that it is ready for pairing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?