Micro Module Shades Control (Puck)
- Remove the rocker from the Wireless switch.
- Short press the top-right push button 5 times in quick succession on the Wireless switch.
-
Follow either of the options to pair the Puck:
WARNINGHAZARD OF ELECTRIC SHOCK- Observe the regulations for working on live parts.
- Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.- Short press the Setup/Reset button 5 times in quick succession on the Puck.
- Short press the right mechanical push button for 5 times in quick succession.
The status LED blinks green on the Puck.NOTE: If the Puck is located behind the mechanical double push button, the status LED is not visible.The shutter moves up and down for a few times. The status LED stops blinking green on the Wireless switch and the Puck. The Puck can now be controlled by the Wireless switch.