DUG_Odace_Wireless Switch_WH-04

Removing configured Action/Moment

You can remove the configured Action or Moment from the Wireless switch key.

To remove the configured Action/Moment:

  1. On the Control tab, tap All devices or the room tab where the Wireless switch is located.

  2. Tap the key with the Action/Moment you want to remove, and then tap Delete > YES, I’M SURE to remove it from the Wireless switch key.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?