DUG_Odace_Wireless Switch_WH-04

Removing the device from the system

You can remove the Wireless switch from the Wiser system.
  1. On the Home screen, tap .
  2. Tap Devices > 2-gang Connected Wireless Switch > Delete (A).

NOTE: By removing the device, it is reset to factory default.
TIP: If the device is still in the system, reset the device manually. Refer to reset the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?