DUG_Odace_Wireless Switch_WH-04

Identifying the device

You can identify a Wireless switch among the other available devices in the room.

To identify the Wireless switch:

  1. Remove the rocker.

  2. Short press the push button (A) 3 times in quick succession.

    The Wireless switch wakes up for a minute and the status LED blinks green 5 times and then stops.

  3. On the Home screen, tap > Devices > 2-gang Connected Wireless Switch > Identify (A).

    The status LED blinks green upon successful identification of the Wireless switch.

    NOTE: It can take up to a minute for the Wireless switch to indicate the status LED.
  4. Tap OK when you have finished identifying the Wireless switch.

  5. Assemble the rocker on the Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?