DUG_PowerTag-E_WH-10

Insights

The Insights provides information on the annual bill for the tariff set. It helps to keep track of your energy.
To know detailed information about insights, refer to Insights.
To view insights:
  1. On the bottom navigation bar, tap > Insights > Energy costs (A).

  2. Select a time period to view the cost consumption.

    • Days

    • Months

    • Years

  3. Tap My savings (B) to view savings and earning history.

    IMPORTANT: My savings is available only in the following scenarios:
    • if you have installed PowerTag on solar or solar with battery (combo).

    • if you have enabled Wiser Home AI feature. For more information, refer to Wiser Home AI.

    NOTE: Please read the description below the images.

    Energy costs with PowerTag installed for Grid and loads

    Energy costs with PowerTag and solar

    Energy costs with PowerTag, Solar and Wiser Home AI

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?