DUG_PowerTag-E_WH-10

Live

Using Wiser Home app, you can view the live data of power flow in your house (Grid import and export).
To view live data:
IMPORTANT: It is necessary to install PowerTag on Grid and additional power sources such as Solar, Solar and Battery to have accurate data of powerflow.
  1. On the bottom navigation bar, tap .
  2. Tap Live.
    • Grid import: The live graph shows the real-time electricity pricing throughout the day. You can interact with the graph to see when the most expensive times are based on your tariff.
      NOTE: This graph is displayed only if you set your tariff to Peak/Off-Peak or Dynamic. Refer to Setting Tariff
       
    • Grid import and export (Applicable for Grid with On Grid solar system): The grid consumption with loads is represented in blue and the excess energy of solar production sold is represented in green.

      The excess energy of solar production sold is represented in green


    • Grid, Solar and Battery
      • Grid: Represented in blue.

      • Solar (PV): Represented in green.

      • Battery: Represented in grey

      Scroll down to view the graph.

      NOTE: Ensure to pair the Schneider Inverter and Boost in daylight to have the PV equipment (Green) to be available in Live.

      • Consumption total: It shows the total energy consumption in kWh.

      • Solar production: It shows the energy produced by the solar system in kWh.

      • Self-sufficiency: It shows the percentage of energy produced by the solar system that is consumed by the household.

      • % of production used: It shows the percentage of solar energy that is used.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?