DUG_Renova - ZB Thermostat 16 A_WH-01

Configuring the device

IMPORTANT: The temperature data from the sensor will be used as an input for the heating system of the room. If a room has multiple temperature measuring devices (Room Thermostat, , Connected Thermostat (2 A or 16 A) or ), the system calculates the average temperature measured from the devices to control the heating based on the overall temperature of the room.
For more details, refer to the .
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?