DUG_Renova - ZB Thermostat 16 A_WH-01

Relay Cycle Time

In advanced settings, you can choose Relay Cycle Time (A). This setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle time may be more appropriate for slow heating surfaces, such as a concrete floor. A short cycle time is more appropriate for faster heating surfaces, such as an electric panel heater.

For example, 20 mins = three cycle per hour.
NOTE: A relay cycle time can be viewed only when the output relay is on.

Tap Relay Cycle Time:
  • 5 mins

  • 10 mins

  • 20 mins

  • 30 mins

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?