DUG_Renova - ZB Thermostat 16 A_WH-01

Setting the device manually

As a standalone thermostat, you can set the following settings and operating parameters.
Preset Configuration Sensor
type
selection
Floor
calibration
setting
Max
guard
temp.
setting
Boost
mode
P1 Heat Pump/Oil Boiler x x x ü
P2 Hydronic Radiator/Gas Boiler x x x ü
P3 Hydronic Underfloor x x x ü
P4 Electrical Radiator x x x ü
P5 Electrical Underfloor (Without floor limits) x x x ü
P6 Electrical Underfloor (With floor limits) ü ü ü ü
P7 Hydronic Underfloor ü ü ü ü
P8 Electrical Underfloor ü ü ü ü
P9 Regulator Mode (output displayed is based on percentage) x x x ü

Refer the following topics for more information on these settings:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?