Device presetting
PI (Proportional and Integral) controller: It is a widely used control method. It minimizes the error between the desired setpoint and the actual value by applying feedback-based corrections.
You can choose one preset configuration:
| Preset | Configuration | Control type / Set point range | Cycle time (min) |
| P1 | Heat Pump/Oil Boiler | Room
Control 4 °C ~ 30 °C |
20 |
| P2 | Hydronic Radiator/Gas Boiler | 10 | |
| P3 | Hydronic Underfloor | 10 | |
| P4 | Electrical Radiator | 10 | |
| P5 | Electrical Underfloor (Without floor limits) | 10 | |
| P6 | Electrical Underfloor (With floor limits) | 10 | |
| P7 | Hydronic Underfloor | Floor
Control 10 °C ~ 40 °C |
10 |
| P8 | Electrical Underfloor | 10 | |
| P9 | Regulator Mode (output displayed is based on percentage) | Floor
Control 0 ~ 10 (0% ~ 100%) |
30 |
Cycle time: The Cycle Time setting defines the duration of each on/off cycle for the output relay. Within a cycle time, the relay cycle (On/Off switching action) operates based on the demand setpoint.
A longer cycle time may be more appropriate for slow heating surfaces, such as concrete floors. A short cycle time is more appropriate for faster heating surfaces, such as electric panel heaters.
Initial preset configuration
(by default):
When the thermostat
is powered on for the first time or immediately after a factory reset,
the Dot-matrix LED displays following default presets.
-
P5 flashes if there is no external sensor connected.
-
P8 flashes if there is any external sensor connected.
To modify the default preset value:
-
Press O and + buttons simultaneously for 10 seconds to enter the preset changing mode
-
Press + button to increase the preset value from P1 to P2.
-
Press – button to decrease the preset value from P2 to P1.
For example, when + button is pressed, preset P1 becomes P2, continue to press the + button, and the preset changes to P3, P4...P9.
Similarly, when – button is pressed, preset P9 changes to P8, continue to press the – button, preset changes to P7, P6...P1.
To confirm the preset selection:
-
Select the preset that meets your needs using the +/- buttons.
-
Press and hold O button for more than 1 second to confirm the selection.
For example, P1 is confirmed.
-
Cycle Time : 20 mins
-
Valve Protection : Off