Showing 1,031 - 1,040 of 1,622 results

Page 104 of 163
  • Changing the orientation of light sensors

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    Changing the orientation of light sensors Changing the orientation of light sensors Changing the orientation of light sensors You can change the orientation of the light sensors in the Wiser Home app. To change the orientation of the light sensors: In the Seasonal Comfort Mode set-up page, tap Light (LUX) sensors. Tap to see the available light sensors in Wiser Home app. Select the orientation in which the light sensors are facing and tap Set.
  • Changer l’orientation et l’emplacement des volets

    Wiser micromodule pour volet roulant – Guide de l'utilisateur de l’appareil Wiser Home

    : Dans la page de configuration du Mode Confort Saisonnier, appuyez sur Volets. Mettez à jour l’orientation des volets et appuyez sur Enregistrer. Si un volet recouvre une porte, appuyez sur Oui, j’ai des volets sur une porte pour définir son emplacement. Si aucun volet ne recouvre une porte, appuyez sur Non. Sélectionnez les volets couvrant les portes dans la liste (A) et appuyez sur Terminer.
  • Changing the shutter orientation and location

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    Mode set-up page, tap Shutters. Update the orientation of the shutters and tap Set. If any shutter is covering a door, tap Yes I have shutters over a door to define its location. If no shutters cover a door, tap No. Select the shutters covering the doors from the list (A) and tap Finish.
  • Changing the shutter orientation and location

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    Mode set-up page, tap Shutters. Update the orientation of the shutters and tap Set. If any shutter is covering a door, tap Yes I have shutters over a door to define its location. If no shutters cover a door, tap No. Select the shutters covering the doors from the list (A) and tap Finish.
  • About the device

    LK® One Wiser Motion Sensor with Switch 10A – Wiser Home Device user guide

    Home control: To control the motion sensor switch through the Wiser Home app you will need the Wiser Hub. Direct operation: The motion sensor switch can always be controlled directly on-site. You can also connect any number of mechanical push-buttons. Functions Detection range. Automatic mode, manual operation.
  • Changer l’orientation des capteurs de luminosité

    Unica - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    la page de configuration du Mode Confort Saisonnier, appuyez sur Capteurs de luminosité (LUX). Appuyez sur pour voir les capteurs de luminosité disponibles dans l’application Wiser Home. Sélectionnez l’orientation dans laquelle les capteurs de luminosité sont installés et appuyez sur Enregistrer.
  • Changing the orientation of light sensors

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    Changing the orientation of light sensors Changing the orientation of light sensors Changing the orientation of light sensors You can change the orientation of the light sensors in the Wiser Home app. To change the orientation of the light sensors: In the Seasonal Comfort Mode set-up page, tap Light (LUX) sensors. Tap to see the available light sensors in Wiser Home app. Select the orientation in which the light sensors are facing and tap Set.
  • Schedules

    Wiser Home – System User Guide (France)

    schedule. For a detailed understanding of which action/control mode takes precedence over others, refer to Understanding Control Mode Priorities . Schedules are created and edited on the Automation screen (A) Tap a Schedule to navigate to the Schedule details. Schedule details: A Device type A Schedule can
  • Création d’un programme/évènement

    Odace - Thermostat connecté filaire 2 A – Guide de l'utilisateur de l’appareil Wiser Home

    pour ajouter un évènement: Sélectionnez la température (par exemple 16°C). Quand vous placez le curseur au bas de la barre pour le programme, le mode Protection contre le gel est activé lorsque le programme commence.En mode Protection contre le gel, le système maintient la température dans la pièce à 5
  • Creating a Schedule/Event

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    schedule, Frost Protection Mode will activate when the schedule begins. In Frost Protection Mode, the system maintains the room temperature at 5 °C to prevent freezing. WHEN: Set the time for the event (for example 12:00) You can create a maximum of 8 events per day. Copy Schedule: You can tap to copy
Page 104 of 163