DUG_Exxact - Blind Control Switch_WH-01

Changing the orientation of light sensors

You can change the orientation of the light sensors in the Wiser Home app.

To change the orientation of the light sensors:
  1. In the Seasonal Comfort Mode set-up page, tap Light (LUX) sensors.
  2. Tap to see the available light sensors in Wiser Home app.
  3. Select the orientation in which the light sensors are facing and tap Set.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.