DUG_Exxact - Blind Control Switch_WH-01

Changing the shutter orientation and location

You can change the orientation and location of the shutter in Wiser Home app.

To change the orientation and location of the shutters:
  1. In the Seasonal Comfort Mode set-up page, tap Shutters.
  2. Update the orientation of the shutters and tap Set.
  3. If any shutter is covering a door, tap Yes I have shutters over a door to define its location.
    NOTE: If no shutters cover a door, tap No.
  4. Select the shutters covering the doors from the list (A) and tap Finish.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.