Showing 251 - 260 of 1,457 results

Page 26 of 146
  • Odace - Connected Multiwire Universal Push-button Dimmer LED Wiser Home Device user guide

    ). – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc
  • LK® One Wiser Multiwire LED Rotary Dimmer Wiser Home Device user guide

    . Tap Add conditions (B) and select any of the following (C). – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger
  • Wiser Micro Module Dimmer Wiser Home Device user guide

    status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. Refer to the AwayMode topic in the respective System User Guide. NOTE: Maximum 10 conditions
  • Creating an automation

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    condition: This triggers an action when at least one condition is met. To add condition, tap Add conditions and select any of the following: Device status change (Select the device) Away Mode (Enable or Disable) Max. of 10 conditions can be added. To remove an added condition, swipe left and tap (D). To
  • Wiser Home System User Guide (Belgium)

    .....................................................................................................50 Away Mode ........................................................................................50App Settings
  • Abwesenheitsmodus

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

  • Wiser Window/Door Sensor Wiser Home Device user guide

    change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information about AwayMode, refer to the system user guide. e.g. Good Morning If When
  • Boost Mode

    Wiser Home – System User Guide (France)

    Boost Mode Boost Mode Boost Mode Boost Mode will apply a boost of +2 °C for one hour to every room in the system. On the Automation Screen: Tap Boost All. To end boost mode earlier, tap Cancel all overrides.
  • Comfort Mode

    Wiser Home – System User Guide (France)

    Comfort Mode Comfort Mode Comfort Mode Comfort Mode is a smart feature that helps ensure the set-point temperature is reached by the time the heating is scheduled to turn ON. It enhances thermal comfort by adjusting the setpoint ahead of schedule, ensuring the room reaches the desired temperature
  • Comfort Mode

    Wiser Home – System User Guide (Denmark)

    Comfort Mode Comfort Mode Comfort Mode Comfort Mode is a smart feature that helps ensure the set-point temperature is reached by the time the heating is scheduled to turn ON. It enhances thermal comfort by adjusting the setpoint ahead of schedule, ensuring the room reaches the desired temperature
Page 26 of 146