DUG_SysM - Connected Thermostat 2 A, ZB_WH-07

Creating an automation

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser app, you can create automations based on your needs.
NOTE: To create and save automation, at least one condition and action must be added.
To create an automation:
  1. On the Home page, tap .
  2. Go to Automation > + to create an automation.
  3. Tap If (A) and select any of the following conditions to meet (B):
    • All conditions: This triggers an action only when all conditions are met.
    • Any condition: This triggers an action when at least one condition is met.
  4. To add condition, tap Add conditions and select any of the following:
    • Device status change (Select the device)
    • Away Mode (Enable or Disable)
    NOTE: Max. of 10 conditions can be added.
    NOTE: To remove an added condition, swipe left and tap (D).
  5. To set a specific time for your automation, tap When > Add time and select any of the following:
    • Specific time of the day: Sunrise, Sunset, Custom
    • Period of time: Daytime, Nighttime, custom
    NOTE: To remove a specific time, swipe left and tap (E).
  6. To add an action, tap Then > Add an action and select any of the following (F):
    NOTE: Max.of 10 actions can be added.
    • Control a device: Select a devices that you want to trigger.
    • Send notification: Turn on the notification for the automation.
    • Activate a moment: Select the moment that you want to trigger.
    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.

    NOTE: To remove an action, swipe left on the action and tap (G).
  7. Enter the automation name (H) and tap Save.

    You can choose the icon from the list that best represents your automation by tapping .

    Once the automation is saved, it is visible on the Automation tab. Using the (I) you can enable and disable the automation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.