Showing 3,341 - 3,350 of 9,859 results

Page 335 of 986
  • About the Document

    Exxact - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    , troubleshooting, and technical specifications to ensure optimal performance and integration within a smart home environment. Validity Note The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate
  • Funcionamiento del interruptor de relé

    Sistema M y sistema D - Módulo soporte de tecla simple/doble conectado – Guía del usuario del dispositivo Wiser Home

  • Identificar o dispositivo

    Micromódulo Variador Wiser – Guia do utilizador do dispositivo Wiser Home

    Identificar o dispositivo Identificar o dispositivo Identificar o dispositivo Através da aplicação Wiser Home, identifique o relé entre os dispositivos disponíveis numa casa. No ecrã Inicial, toque em . Toque em Dispositivos Micromódulo variador Identificar (A). O LED de estado pisca a vermelho e
  • Identificar o dispositivo

    Sensor de fumo 230V Wiser – Guia do utilizador do dispositivo Wiser Home

    Identificar o dispositivo Identificar o dispositivo Identificar o dispositivo Através da aplicação Wiser Home, identifique o dispositivo entre os sensores de fumo disponíveis numa casa. No ecrã inicial, toque em . Toque em Dispositivos Identificar (A). O LED do sensor de fumo pode demorar até 60
  • Setting the device location

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Setting the device location Setting the device location Setting the device location You can add your Wireless Switch to any room (such as bedroom, living room, dining room etc.). To add a Wireless Switch to a room: On the Home screen, tap . Tap Devices 2-gang Connected Wireless Switch Location (A) to assign the Wireless Switch to an existing room or a new room (B) and tap Submit.
  • Pairing the device with Wiser Hub

    System M and System D - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are
  • Emparejamiento del dispositivo Airzone con el Wiser Hub

    Plenum Airzone y Aidoo Pro - Aire acondicionado – Guía del usuario del dispositivo Wiser Home

    : para emparejar los dispositivos Airzone con el Wiser Hub: Wiser Hub y los dispositivos Airzone deben actualizarse a la versión más reciente del sistema. Todos deben estar conectados a la misma red Wi-Fi. La aplicación Airzone Cloud puede utilizarse para conectar dispositivos Airzone a una red
  • Navigating the Floorplan

    Wiser BMS – Building Management System – User Guide

    also check the temperature settings, turn devices ON or OFF remotely, and create schedules. On the Home screen, click Floorplan. On the left pane, you can see the following options: Building Overview Floorplan Building Overview The Building Overview displays a complete image of the building. When
  • Sistema M y sistema D - Interruptor inalámbrico de una/dos teclas conectado Guía del usuario del dispositivo Wiser Home

    dispositivo. 10/2025 www.se.com https://www.se.com Información legalLa información proporcionada en este documento contiene descripciones generales,características técnicas o recomendaciones relacionadas con productos osoluciones. Este documento no pretende sustituir a un estudio detallado o un plan
  • Välja plats för enheten

    Wiser dimmerpuck LED – Användarhandbok för Wiser Home-enhet

    Välja plats för enheten Välja plats för enheten Välja plats för enheten Använd Wiser Home-appen och lägg till pucken i valfritt rum (t.ex. vardagsrum, sovrum, kök osv.). På startskärmen trycker du på . Tryck på Enheter Mikromoduldimmer Plats (A) för att tilldela pucken till ett befintligt rum eller
Page 335 of 986