Showing 3,991 - 4,000 of 9,859 results

Page 400 of 986
  • Wiser Home IA

    Wiser Home – Guía del usuario del sistema (España y Portugal)

    Wiser Home IA Wiser Home IA Wiser Home IA Wiser Home IA es una función que permite a los usuarios ahorrar en costes de electricidad registrando dispositivos de alto consumo energético, como cargadores de EV (EVlink Home Smart, Schneider Charge) o calderas de agua resistivas (controladas con un
  • Configuring the seasonal comfort mode

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    configuring the seasonal comfort mode. Define the orientation in which the shutters are installed at home: Select the orientation in which each shutter is installed at home and tap Next. If any shutter is covering a door, tap Yes I have shutters over a door. If no shutter is covering a door or you have an
  • Pairing the device with the Wiser Hub

    LK® One Wiser Motion Sensor with Switch 10A – Wiser Home Device user guide

    incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid. (B): Tap this option if you
  • Pairing the device with the Wiser Hub

    LK FUGA® Wiser wireless dimmer – Wiser Home Device User Guide

    Home app to access your camera. Then, scan the QR code located on the device. If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't
  • Remover o dispositivo do sistema Wiser

    Unica - Comando de estores conectável – Guia do utilizador do dispositivo Wiser Home

    > Interruptor de controlo dos estores ou Lâminas dos estores > Eliminar (A). Ao remover o dispositivo irá reiniciar o interruptor do controlo dos estores O LED começa a piscar a âmbar, indicando que o interruptor de controlo dos estores está pronto para o emparelhamento. Se surgir algum problema durante o emparelhamento ou a reinicialização do interruptor de controlo do estores, consulte Repor o dispositivo.
  • Tekniset tiedot

    Exxact – Multiwire LED-säädin ZB – Wiser Home -laitteen käyttöopas

    Tekniset tiedot Tekniset tiedot Tekniset tiedot Nimellinen teho Kuorman tyyppi Kuorman nimi Kuorman arvo 2‑johtiminen (ilman nollajohdinta) 3-johtiminen (nollajohtimen kanssa) LED 7–130 W (enint. 0,8 A) 7–80 W (enint. 0,5 A) 0–130 W (enint. 0,8 A) 0–80 W (enint. 0,5 A) Hehkulamppu 14–200 W 0–200 W
  • Aikataulun määrittäminen

    Exxact - Pistorasia 1-os. Zigbee – Wiser Home -laitteen käyttöopas

  • Zeitplan einrichten

    System M und System D - Connected Taster-Modul, 1fach/2fach – Wiser Home Geräte-Benutzerhandbuch

    Zeitplan zu erstellen. Geben Sie den Namen des Zeitplans ein (A). Wählen Sie im Menü TYP die Option Leuchten (B). Im GILT FÜR Menü, auswählen Dimmer (C) von den aufgelisteten Geräten. Tippen Sie auf Erstellen, um Ereignisse einzurichten. Wählen Sie im Menü EREIGNISSE einen Tag aus und tippen Sie dann
  • Zeitplan erstellen

    Wiser Smart Plug – Wiser Home Geräte-Benutzerhandbuch

    Zeitpläne . Geben Sie einen Namen des Zeitplans ein (A). Wählen Sie einen Gerätetyp (B). Wählen Sie die Geräteliste (C), für die der Zeitplan gelten soll. Tippen Sie auf Erstellen. Tippen Sie auf , um ein Ereignis hinzuzufügen. Wählen Sie einen Zustand (Ein/Aus) (D), einen Zeitraum (E) und tippen Sie auf
  • Pairing the device with the Wiser Hub

    Wiser Plug – Wiser Home Device User Guide

    . You can also navigate by tapping Control > > Appliances > Smart Plug. The next screen shows the joining process of the Plug. Press and hold the ON/OFF button for 2 seconds on the Plug until the LED flashes blue. The Plug is now successfully joined. Once the device is joined, tap (A) and
Page 400 of 986