DUG_LK FUGA Wiser wireless dimmer_WH-00

Pairing the device with the Wiser Hub

  1. On the Home screen, tap .
  2. Tap Devices > > Lights > Combi Dimmer.
    TIP: You can also navigate by tapping Control > > Lights > Combi Dimmer.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.

  4. Tap Next, short press the top-left push button 3 times (< 0,5 s) and make sure that the LED blinks amber.
    Wait for a few seconds until the LED turns green and the app confirms that the device has been joined.
    NOTE: If the LED is not blinking amber, see the instructions by tapping LED not blinking amber? or refer to Troubleshooting.
  5. Tap to enter the device name.
  6. Tap Next, assign the device to a new or existing room, and then tap Submit.
    IMPORTANT: The next screen shows the Device Settings screen, where you have an option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information, refer to Configuring the device section.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    TIP: The dimmer is now added with an onboarding tip on the Control tab under the All and Room tabs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.