Showing 4,421 - 4,430 of 9,846 results

Page 443 of 985
  • Mise hors service d’un système Wiser

    Wiser Home – Guide de l’utilisateur du système (France)

  • Selecting the mounting location

    Wiser Home – System User Guide (France)

    Selecting the mounting location Selecting the mounting location Selecting the mounting location The Hub is the controller of the system and must be within a range of all devices in order for the system to work properly. The ideal location for the Hub is determined by the following: Layout of the
  • Informações de segurança

    Unica - Botão variador de luz LED conectável – Wiser Home Dispositivo Guia do utilizador

    especiais podem aparecer ao longo deste manual ou no equipamento para avisar de potenciais perigos ou para chamar a atenção para informação que esclareça ou simplifique um procedimento. O aditamento de um dos símbolos a um rótulo de segurança «Perigo» ou «Aviso» indica a existência de um perigo elétrico que
  • Déconnexion d’un appareil secondaire

    Wiser détecteur de fumée sur batterie – Guide de l'utilisateur de l’appareil Wiser Home

  • Commissioning Wiser Hub to Matter Ecosystem

    Wiser Home – System User Guide (Spain and Portugal)

    Connections Matter. Tap Add a new connection. A screen will appear with instruction how to join the Matter network using the QR code on the Wiser Hub 2 nd Generation / Wiser HubR 2 nd Generation or the pairing code. Tap Allow Matter Joining and wait for the hub to connect to the Matter network (this may
  • Notifications and Alarms

    Wiser Home – System User Guide (Belgium)

    specific device. You can select the Notifications and Alarms in the Account options of the Settings menu. Notifications and Alarms settings are saved for an account in the Wiser cloud. Changes to one mobile device affect all mobile devices using the same account. Tap Notifications and Alarms (A
  • Commissioning Wiser Hub to Matter Ecosystem

    Wiser Home – System User Guide (Belgium)

    Connections Matter. Tap Add a new connection. A screen will appear with instruction how to join the Matter network using the QR code on the Wiser Hub 2 nd Generation or the pairing code. Tap Allow Matter Joining and wait for the hub to connect to the Matter network (this may take up to 15 minutes). Choose
  • Informações técnicas

    Sensor de fumo 230V Wiser – Guia do utilizador do dispositivo Wiser Home

    Informações técnicas Informações técnicas Informações técnicas Alimentação elétrica 110-240 V CA, 50/60 Hz Vida útil da bateria de reserva 10 anos Corrente de funcionamento ≤ 60 mA Tipo de deteção Fotoelétrico. Este alarme NÃO contém material radioativo. Temperatura de funcionamento 0 °C a 45 °C
  • Déconnexion d’un appareil secondaire

    Wiser détecteur de fumée connecté sur secteur 230V – Guide de l'utilisateur de l’appareil Wiser Home

  • About the document

    PowerTag Energy – Wiser Home Device user guide

    accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information. For your safety HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH Safe electrical installation must be carried out only by skilled
Page 443 of 985