Showing 4,431 - 4,440 of 9,846 results

Page 444 of 985
  • Anti-Tripping Management

    Schneider Charge – Wiser Home Device user guide

    Anti-Tripping Management Anti-Tripping Management Anti-Tripping Management The Anti-Tripping Management prevents the circuit breaker from tripping by switching off the load or reducing the power of the load. This keeps the total consumption of the system under a defined limit. The limit value is
  • EcoWatt

    Wiser Home – System User Guide (France)

    , updated every hour, with 48 hours forecast data. EcoWatt allows you to know the moments when eco-gestures have the greatest impact on the electrical system. EcoWatt feature is applicable only for customers in France. Features of EcoWatt: Send notifications about the grid status. Send alerts if there is a
  • EcoWatt

    EcoWatt – User Guide

    , updated every hour, with 48 hours forecast data. EcoWatt allows you to know the moments when eco-gestures have the greatest impact on the electrical system. EcoWatt feature is applicable only for customers in France. Features of EcoWatt: Send notifications about the grid status. Send alerts if there is a
  • Informações técnicas

    Controlador temperatura 16A Wiser – Guia do utilizador do dispositivo

    ) indutiva para carga piloto (FP) Não adequado para aquecedores de rodapé. Classificação IP: IP44 Terminais e fiação: Adequado para tamanhos de condutor 1,0- 2,5 mm² Comprimento da parte descarnada 6,5 mm Temperatura de funcionamento: 0 °C a 60 °C Temperatura de armazenamento: -20 °C a 65 °C Classe de
  • Pairing 2-gang Wireless switch with 2 Micro Module Dimmers (Pucks)

    Wiser Micro Module Dimmer – Wiser Home Device user guide

    pairing mode. The pairing mode will be active for about a minute. Short press the upper right push button 5 times in quick succession on the Wireless switch. The status LED blinks green. HAZARD OF ELECTRIC SHOCK Observe the regulations for working on live parts. Only actuate the device buttons using
  • Konfigurieren – Pauschaltarif

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    , folgen Sie der Menünavigation, wenn Sie den Tarif ändern müssen.Tippen Sie im Startbildschirm auf Energiemanagement Tarif Elektrizität. Tippen Sie auf (A) und wählen Sie Pauschale. Tippen Sie auf (B), um die Vertragliche Strombegrenzung festzulegen. Vertragliche Strombegrenzung ist bereits beim Koppeln
  • Resolução de problemas no Quick Home Connect

    Unica - LED Variador de Luz Conectável – Manual do utilizador do dispositivo doméstico Wiser

    Resolução de problemas no Quick Home Connect Resolução de problemas no Quick Home Connect Resolução de problemas no Quick Home Connect Problema Causa possível Solução O LED fica âmbar no dispositivo. O emparelhamento não foi concluído e voltou à predefinição de fábrica. Volte a emparelhar o
  • Dépannage

    Mureva EVlink – Guide de l'utilisateur de l'appareil domestique Wiser

    Dépannage Dépannage Dépannage Symptôme Cause possible Solution L’appairage a échoué ou a dépassé le temps imparti à cet effet. Aucun appui sur le bouton d’appairage dans les 5 minutes suivant la mise sous tension. Coupez l’alimentation de la prise EV en mettant le disjoncteur hors tension/sous
  • Restablecimiento del PIN con la aplicación eSetup

    Schneider Charge – Guía del usuario del dispositivo Wiser Home

    creará una red inalámbrica temporal, que estará activa durante 4 min. Si la luz indicadora LED lateral está apagada, apague la estación de carga y vuelva a encenderla para reactivar el botón lateral. En la aplicación, pulse Sí, está respirando verde, y realice uno de los siguientes métodos para
  • Setting Tariff

    Wiser Home – System User Guide (Germany, Austria)

    Setting Tariff Setting Tariff Setting Tariff You can set tariff in the Wiser Home app to access your energy cost and billing data. The Tariff option available only if you have installed the following energy monitoring device installed at your home. EVlink Home Smart Schneider Charge Wiser 16 A
Page 444 of 985