Showing 501 - 510 of 1,457 results

Page 51 of 146
  • Changing the device from 1-gang to 2-gang

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Changing the device from 1-gang to 2-gang Changing the device from 1-gang to 2-gang Changing the device from 1-gang to 2-gang You can change the Wireless switch mode from 1-gang to 2-gang before you pair your device to the Hub/Gateway. The Wireless switch is in 1-gang mode by default. Follow the
  • Boost-Modus

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

  • Modo de potenciación

    Wiser Home – Guía del usuario del sistema (España y Portugal)

  • Setting the room temperature manually

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    the temperature. In the thermostat, press “ -” touch button to decrease the temperature. When the system is in heating mode and the setpoint is higher than the current room temperature then the demand LED is lit Red to show the heating mode is active. When the system is in cooling mode and the setpoint is lower than the current room temperature then the demand LED is lit Blue to show cooling mode is active.
  • Troubleshooting

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    button 3 times, the device LED blinks red/green for 30 s. Pairing mode has changed to Bluetooth mode. Press the top-left push button on the device 3 times, hold it for 20 s until the LED blinks red, and the device reboots into the correct mode (Zigbee mode). Unable to configure a group, edit, or delete
  • Setting the room temperature manually

    System M und System D - Connected Raumtemperaturregler 2 A, ZB – Wiser Home Geräte-Benutzerhandbuch

    : In the “ clockwise” direction to increase the temperature. In the “ anti-clockwise” direction to decrease the temperature. When the system is in heating mode and the setpoint is higher than the current room temperature then the demand LED is lit Red to show the heating mode is active. When the system is in cooling mode and the setpoint is lower than the current room temperature then the demand LED is lit Blue to show cooling mode is active.
  • Setting the room temperature manually

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    : In the “ clockwise” direction to increase the temperature. In the “ anti-clockwise” direction to decrease the temperature. When the system is in heating mode and the setpoint is higher than the current room temperature then the demand LED is lit Red to show the heating mode is active. When the system is in cooling mode and the setpoint is lower than the current room temperature then the demand LED is lit Blue to show cooling mode is active.
  • Modes de fonctionnement

    Micromodule chauffage électrique FIP – Guide de l'utilisateur de l’appareil Wiser Home

    l’écran Contrôle de l’appareil, vous pouvez voir la température actuelle. Le mode de fonctionnement actuel indique le mode dans lequel le système fonctionne. Arrêt : Éteint le système, disponible sur l’écran d’ accueil. Chauffage : Le système fonctionne en mode chauffage lorsque la température de
  • LED Indication

    LK FUGA Wiser Multiwire LED Push-button Dimmer – Wiser Home Device user guide

    LED Indication LED Indication LED Indication Pairing User Action LED Indication Status Press the push button 3 times LED blinks amber per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning off. Resetting User Action LED Indication
  • Setting the room temperature manually

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    : In the “ clockwise” direction to increase the temperature. In the “ anti-clockwise” direction to decrease the temperature. When the system is in heating mode and the setpoint is higher than the current room temperature then the demand LED is lit Red to show the heating mode is active. When the system is in cooling mode and the setpoint is lower than the current room temperature then the demand LED is lit Blue to show cooling mode is active.
Page 51 of 146