DUG_SysM - Connected Thermostat 2 A, ZB_WH-07

Setting the room temperature manually

The room temperature can be increased/decreased manually by rotating the rotary push-button of the thermostat.
Prerequisite: Select the Preset.

Rotate the thermostat rotary push-button:
  • In the “clockwise” direction to increase the temperature.

  • In the “anti-clockwise” direction to decrease the temperature.

NOTE:
  • When the system is in heating mode and the setpoint is higher than the current room temperature then the demand LED is lit Red to show the heating mode is active.

  • When the system is in cooling mode and the setpoint is lower than the current room temperature then the demand LED is lit Blue to show cooling mode is active.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.