DUG_Odace - Thermostat 2 A_WH-06

Setting the room temperature manually

The room temperature can be increased/decreased manually by using touch button on the thermostat.
Prerequisite: Select the Preset.

  • In the thermostat, press “+” touch button to increase the temperature.

  • In the thermostat, press “-” touch button to decrease the temperature.

NOTE: When the system is in heating mode and the setpoint is higher than the current room temperature then the demand LED is lit Red to show the heating mode is active.
NOTE: When the system is in cooling mode and the setpoint is lower than the current room temperature then the demand LED is lit Blue to show cooling mode is active.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?