Showing 5,211 - 5,220 of 9,846 results

Page 522 of 985
  • Weather and Heating

    Wiser Home – System User Guide (Spain and Portugal)

    Weather and Heating Weather and Heating Weather and Heating (A) The weather can have a big impact on how your heating system performs. We take into account the thermal efficiency of your home and the outdoor temperature, so we can save you as much as possible. Heating time The green bars show an
  • Historik

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    . På trycker du på Historik för att visa Energikällor. Här visas den totala energi som genereras och förbrukas. Om inga energikällor spåras kommer energikälldata inte att vara tillgängliga. Du kan ändra den visade tidsramen (timmar, dagar, månader och år) genom att trycka på (A). Gröna staplar visar
  • Redigering af en automatisering

    Wiser Home – Systembrugervejledning (Danmark)

    Redigering af en automatisering Redigering af en automatisering Redigering af en automatisering På skærmen Automatisering (A): Tryk på automatiseringen, du vil redigere (B). På skærmen Redigér automatisering kan du: Ændre ikonet. Omdøbe automatiseringen. Reducere betingelsen, tiden eller handlingen
  • Editing an automation

    Wiser Smoke Alarm - 230 V – Wiser Home Device user guide

    the settings. To remove a condition, slide the condition towards left and then tap (A) to delete it. Tap ⊕ Add conditions (B) to add new condition. To change the order of actions, tap the Then option, and hold an action, then drag and drop to the desired position. Tap Save to save the changes.
  • Turning On/Off device using app

    Exxact - Connected Motion Sensor with Multiwire Dimmer – Wiser Home Device user guide

    Turning On/Off device using app Turning On/Off device using app Turning On/Off device using app On the Control tab, tap All devices or the room tab where the device is located. Tap (A) to turn on/off the device. The Control tab will not be visible if you have only a single device in the Wiser System. All functions will be accessible through the Home screen.
  • Resetting the device

    Unica - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    successful reset, the LED stops blinking. Then, the device restarts and blinks green for a few seconds. After reset, the LED turns amber indicating that it is ready for pairing.
  • Away Mode

    LK FUGA® Wiser wireless PIR with relay – Wiser Home Device user guide

    Away Mode Away Mode Away Mode Away Mode automatically turns off the Motion Sensor Switch. For example, when you are away from home for a long time, the light should not turn on due to false motion detections. This feature ensures the device remains off even if motion is detected, helping to save
  • Away Mode

    LK FUGA® Wiser wireless PIR dimmer with neutral – Wiser Home Device user guide

    Away Mode Away Mode Away Mode Away Mode automatically turns off the Motion Sensor Dimmer. For example, when you are away from home for a long time, the light should not turn on due to false motion detections. This feature ensures the device remains off even if motion is detected, helping to save
  • Ændring af ikonet og ny tildeling af udstyrstypen

    Wiser Smat Plug 16 A – Brugervejledning til Wiser Home-enheden

    Ændring af ikonet og ny tildeling af udstyrstypen Ændring af ikonet og ny tildeling af udstyrstypen Ændring af ikonet og ny tildeling af udstyrstypen Du kan ændre enhedens ikon. Tryk på Hjem skærmen på Enheder Smart Plug. Tryk på ikonet, vælg et ikon for udstyrstypen (A), og tryk på Gem (B). Hvis
  • Identifikation af enheden

    Wiser Smat Plug 16 A – Brugervejledning til Wiser Home-enheden

    Identifikation af enheden Identifikation af enheden Identifikation af enheden Ved hjælp af Wiser Home-appen kan du identificere stikket fra andre tilgængelige enheder i rummet. Sådan identificeres stikket: Tryk på på Hjem-skærmen. Tryk på Enheder Intelligent stik Identificer (A). Denne funktion får
Page 522 of 985