Showing 6,631 - 6,640 of 9,846 results

Page 664 of 985
  • Setting boost mode manually

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

  • Limitations of the Wiser System

    Wiser Home – System User Guide (Sweden, Finland)

    Limitations of the Wiser System Limitations of the Wiser System Limitations of the Wiser System When commissioning a Wiser system, it is important to understand the system limits, such as the maximum number of supported devices. System Limits Maximum number of Devices Zigbee 63 Hub 1 PowerTag E 20
  • Support

    Wiser Home – System User Guide (Sweden, Finland)

    of the Wiser system. Upload Logs This option allows you to upload log files if you have identified any issues in the app. When you tap on the option, a popup will appear, allowing you to describe the issue. Click OK to generate an ID number for this problem, and then contact the Schneider support
  • Support

    Wiser Home – System User Guide (Belgium)

    of the Wiser system. Upload Logs This option allows you to upload log files if you have identified any issues in the app. When you tap on the option, a popup will appear, allowing you to describe the issue. Click OK to generate an ID number for this problem, and then contact the Schneider support
  • Prueba del dispositivo

    Alarma de humo Wiser - 230V – Guía del usuario del dispositivo Wiser Home

    Prueba del dispositivo Prueba del dispositivo Prueba del dispositivo La alarma de humo cuenta con un modo de prueba que ayuda a garantizar el funcionamiento correcto del dispositivo. Se recomienda probar la alarma de humos una vez al mes. Si la alarma de humo se instala en un hogar móvil, se
  • Override modes

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    Override modes Override modes Override modes This mode temporarily overrides the automatic operation of the motion sensor. For example, it allows you to trigger the load for a set period, even if no motion is detected. The motion sensor has two modes that can temporarily override the default
  • Shutter calibration with Wiser app

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    percentage (A). The shutter opens completely and then it reaches to the desired position set in step 2. The shutter is now calibrated. Shutter with tilting slats On the Control tab, tap All devices or the room tab where the device is located. On the device control screen, in the Position tab, drag the
  • Konfigurera UFH-ställdon

    Renova – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enheter

    ihop och tryck sedan på Nästa för att konfigurera golvvärmen. Tryck Utgångsenhet (A) för att öppna rullgardinsmenyn och välj UFH (B) från listan som är ansluten till termostaten. Inbyggt relä är valt som standard som utgångsenhet, det finns inga andra inställningar för det. Tryck på Kanaler (C) och
  • Uso del dispositivo

    Unica - Detector de movimiento con regulador LED conectado – Guía del usuario del dispositivo Wiser Home

    muestra las siguientes opciones: A Pulse para encender/apagar el dispositivo. B Arrastre la barra deslizante hacia arriba/hacia abajo para aumentar/reducir el brillo de su atenuador de movimiento. Para obtener más información, consulte Ajuste del brillo. C Muestra el valor lux actual de la luz presente
  • Gestión del funcionamiento de la persiana sin sensor de temperatura

    Sistema M y sistema D - Módulo soporte de tecla simple/doble conectado – Guía del usuario del dispositivo Wiser Home

    habitación donde no se ha instalado ningún sensor de temperatura. Para definir la temperatura de referencia: En la página de configuración del Modo confort estacional, pulse Otros sensores de habitación. La aplicación Wiser Home muestra las habitaciones sin sensores de temperatura en la lista (A). Seleccione
Page 664 of 985