Showing 7,971 - 7,980 of 9,969 results

Page 798 of 997
  • User interface lock settings

    Wiser Room Thermostat – Wiser Home Device user guide

    control: On the Home screen, tap . Tap Devices Room Thermostat Device lock (A). When the Room Thermostat lock is active, will appear next to the Room Thermostat.
  • Indstilling af gulvsensorens placering

    Wiser gulvvarmestyring/forbindelsesskinne – Brugervejledning til Wiser Home-enheden

    Indstilling af gulvsensorens placering Indstilling af gulvsensorens placering Indstilling af gulvsensorens placering Ved hjælp af Wiser Home-appen kan du indstille gulvsensorens placering. Forudsætning: Tilknyt en kanal til rummet. Sådan indstilles gulvsensorens placering: Tryk på på Hjem-skærmen. Tryk på Enheder Gulvvarme Placering af gulvsensor (A) for at vælge Ikke tilknyttet eller vælge det ønskede rum, hvor gulvsensoren er tilsluttet. Tryk Ok
  • Installera enheten

    Wiser golvvärmeregulator/fördelarpanel – Bruksanvisning för Wiser Home-enhet

    luftfuktighetssensor Systemet kan installeras utan anslutning till en Wi-Fi-router. Vid användning av utförandet Golvvärme uppvärmning/kylning 24 V ser du till att den är ansluten till en 24 V 2,2 A-strömförsörjning (ingår ej)
  • Operating Elements

    Wiser Home – System User Guide (France)

    Operating Elements Operating Elements Operating Elements A Setup Activates the temporary Wi-Fi ® network of the Hub. It is used during the commissioning process and troubleshooting. B Heating Override* Turning on the heating override will turn on the connected heating system for 2 hours regardless
  • Paramétrer l’emplacement du dispositif

    Odace - Interrupteur simple/double sans fil connecté – Guide de l'utilisateur du dispositif Wiser Home

    ’ accueil, appuyez sur . Appuyez sur Equipements Interrupteur double sans fil connecté Emplacement (A) pour affecter l’interrupteur sans fil à une pièce existante ou à une nouvelle pièce (B), puis appuyez sur Envoyer.
  • Removing the device from the system

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    Removing the device from the system Removing the device from the system Removing the device from the system You can remove the Wireless switch from the Wiser system. On the Home screen, tap . Tap Devices 2-gang Connected Wireless Switch Delete (A). By removing the device, it is reset to factory default. If the device is still in the system, reset the device manually. Refer to reset the device.
  • Resetting the device

    Wiser Motion Sensor – Wiser Home Device user guide

    once (>10 s); the LED blinks red after 10 s, then release the function key. Upon successful reset of the sensor, the LED stops blinking. The sensor restarts and blinks green for a few seconds. After reset, the LED turns off to save the battery.
  • Utilisation de l’appareil

    Capteur de fenêtre/porte Wiser – Guide de l'utilisateur de l’appareil Wiser Home

    panneau de commande du capteur, vous pouvez voir les éléments suivants : Statut de la fenêtre/porte (A) Historique (B) Paramètres de l’équipement (C) Ajouter aux favoris (D)
  • Operating the device manually

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    Operating the device manually Operating the device manually Operating the device manually Long press the blind control switch (> 0,5 s) to move the shutter up or down (A). Press (ʌ) to open the shutter. Press (v) to close the shutter. Short press (<0,5 s) to stop the moving shutter (B). For shutter with tilting slats: When the shutter is not moving short press (<0,5 s) the blind control switch to adjust the slat position (C).
  • WLAN-Anmeldeinformationen für Ihr Zuhause ändern

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    Verbindung zum Hub unterbrochen ist, und schlägt Lösungen vor. So ändern Sie die WLAN-Informationen im Hub: Tippen Sie auf WLAN-Router wurde geändert (A). Die App führt Sie durch die Auswahl eines WLAN-Netzwerks und Eingabe des Kennworts.
Page 798 of 997