DUG_Room Thermostat_WH-09

User interface lock settings

Using the Wiser Home app, you can lock the Room Thermostat controls. This prevents children from changing the temperatures in your room when playing with the Room Thermostat.
To lock or unlock the Room Thermostat control:
  1. On the Home screen, tap .
  2. Tap Devices > Room Thermostat > Device lock (A).
    TIP: When the Room Thermostat lock is active, will appear next to the Room Thermostat.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?