Showing 8,661 - 8,670 of 9,886 results

Page 867 of 989
  • Exporting the charge history

    EVlink Home Smart – Wiser Home device user guide

    each charging cycle to see the charging cost of the session. Tap (A) and then tap Export charge history (B) to export the charger history To ensure proper functionality, use the Microsoft-recommended procedure to import the CSV file into Excel. Your history report will be exported in CSV format.
  • Eksport af opladningshistorik

    EVlink Home Smart – Brugervejledning til Wiser Home-enhed

    mere information, se Live. Tryk på på hver opladningscyklus for at se opladningsomkostningerne for sessionen. Tryk på (A), og tryk derefter på Eksporter opladningshistorik (B) for at eksportere opladningshistorikken For at sikre korrekt funktionalitet, skal du bruge den Microsoft-anbefalede procedure til at importere CSV-filen i Excel. Din historikrapport vil blive eksporteret i CSV-format.
  • Configuración de la alarma de sobreconsumo

    Wiser Home – Guía del usuario del sistema (España y Portugal)

    Configuración de la alarma de sobreconsumo Configuración de la alarma de sobreconsumo Configuración de la alarma de sobreconsumo En este tema se explica cómo configurar una alarma de sobreconsumo para un dispositivo. En la página Notificaciones y Alarmas, toque Crear una nueva alarma (A
  • Utilisation de l’appareil

    Wiser micromodule multifilaire pour variateur LED – Guide d'utilisation de l'appareil Wiser Home

    . L’écran de contrôle de l’appareil affiche les options suivantes : A Faites glisser la barre coulissante vers le haut/bas pour augmenter/réduire la luminosité. B Appuyez pour allumer ou éteindre manuellement l’appareil. C Appuyez pour vous rediriger vers l’écran Programme, dans lequel vous pouvez
  • Managing Matter Connection

    Wiser Home – System User Guide (UK, Ireland)

    network and try connecting again. Refer to Commissioning Wiser Hub to Matter Ecosystem to rejoin the matter network. If you want to completely remove the network from the Matter network. Make sure you remove the network from your third-party app as well. Add a new connection: Tap this option to add new connections to the Matter network. Refer to Commissioning Wiser Hub to Matter Ecosystem to add new connection.
  • Energy Dashboard

    Wiser BMS – Building Management System – User Guide

    . Outside Air Temperature. The signature graph, helps you identify abnormalities in the energy consumption of a building. Any abnormalities, indicates an issue in the building, requiring further investigation by the building manager (BM). This ensures that the comfort for the tenants is not hampered. For
  • Replacing the battery

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    cover with your thumb. Slide the battery cover with another thumb to remove. Remove the old battery, then press any push button on the device for a few seconds to reboot it and delete the internal low battery flag. Dispose the used batteries, as per statutory regulations. Insert the battery with plus (+) symbol facing outward Secure the battery cover.
  • Réglage de la sensibilité de détection

    Unica - Détecteur de mouvement avec interrupteur 10 A connecté – Guide de l'utilisateur de l’appareil Wiser Home

  • Fjernelse af enheden fra Wiser-systemet

    Wiser trådløs jalousi styring for indbygning (puck) – Brugervejledning til Wiser Home-enheden

    Fjernelse af enheden fra Wiser-systemet Fjernelse af enheden fra Wiser-systemet Fjernelse af enheden fra Wiser-systemet Ved hjælp af Wiser-appen kan du fjerne Pucken fra systemet. Tryk på på Hjem-skærmen. Tryk på Enheder Lukker Mikromodul-lukker eller Skoddelamel > Slet (A). Pucken nulstilles
  • Indicadores LED

    Controlador temperatura 16A Wiser – Guia do utilizador do dispositivo

    verde Não emparelhado Desligado: aquecimento desligado Laranja constante: aquecimento ligado Modo degradado(sem ligação com o termóstato ou com o gateway) Vermelho intermitente: aquecimento desligado Vermelho constante: aquecimento ligado Teste manual / Forçando Verde intermitente: aquecimento ligado devido a forçamento
Page 867 of 989