UG_Wiser Building Management System_WH-00

Energy Dashboard

The Energy Dashboard provides detailed information on the energy consumption of an entire building. It offers visualizations of energy data through charts and graphs, making complex information easy to understand. This allows you to analyze usage patterns, identify areas for improvement, and track costs.

Here are some examples of energy dashboards.

The below chart explains the Expected consumption vs. Actual consumption.

The below graph explains the total building energy consumption.

The signature graph explains the Building Energy vs. Outside Air Temperature.

The signature graph, helps you identify abnormalities in the energy consumption of a building.

Any abnormalities, indicates an issue in the building, requiring further investigation by the building manager (BM). This ensures that the comfort for the tenants is not hampered.

For example, if the hot water tank is losing heat, it is not normal and should be checked. Additionally, if energy consumption is higher than expected, the BM should investigate the cause.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.