Showing 8,691 - 8,700 of 9,886 results

Page 870 of 989
  • Exporting the charge history

    EVlink Home Smart – Wiser Home device user guide

    each charging cycle to see the charging cost of the session. Tap (A) and then tap Export charge history (B) to export the charger history To ensure proper functionality, use the Microsoft-recommended procedure to import the CSV file into Excel. Your history report will be exported in CSV format.
  • Eksport af opladningshistorik

    EVlink Home Smart – Brugervejledning til Wiser Home-enhed

    mere information, se Live. Tryk på på hver opladningscyklus for at se opladningsomkostningerne for sessionen. Tryk på (A), og tryk derefter på Eksporter opladningshistorik (B) for at eksportere opladningshistorikken For at sikre korrekt funktionalitet, skal du bruge den Microsoft-anbefalede procedure til at importere CSV-filen i Excel. Din historikrapport vil blive eksporteret i CSV-format.
  • Configuración de la alarma de sobreconsumo

    Wiser Home – Guía del usuario del sistema (España y Portugal)

    Configuración de la alarma de sobreconsumo Configuración de la alarma de sobreconsumo Configuración de la alarma de sobreconsumo En este tema se explica cómo configurar una alarma de sobreconsumo para un dispositivo. En la página Notificaciones y Alarmas, toque Crear una nueva alarma (A
  • Utilisation de l’appareil

    Wiser micromodule multifilaire pour variateur LED – Guide d'utilisation de l'appareil Wiser Home

    . L’écran de contrôle de l’appareil affiche les options suivantes : A Faites glisser la barre coulissante vers le haut/bas pour augmenter/réduire la luminosité. B Appuyez pour allumer ou éteindre manuellement l’appareil. C Appuyez pour vous rediriger vers l’écran Programme, dans lequel vous pouvez
  • Managing Matter Connection

    Wiser Home – System User Guide (UK, Ireland)

    network and try connecting again. Refer to Commissioning Wiser Hub to Matter Ecosystem to rejoin the matter network. If you want to completely remove the network from the Matter network. Make sure you remove the network from your third-party app as well. Add a new connection: Tap this option to add new connections to the Matter network. Refer to Commissioning Wiser Hub to Matter Ecosystem to add new connection.
  • Energy Dashboard

    Wiser BMS – Building Management System – User Guide

    . Outside Air Temperature. The signature graph, helps you identify abnormalities in the energy consumption of a building. Any abnormalities, indicates an issue in the building, requiring further investigation by the building manager (BM). This ensures that the comfort for the tenants is not hampered. For
  • Replacing the battery

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    cover with your thumb. Slide the battery cover with another thumb to remove. Remove the old battery, then press any push button on the device for a few seconds to reboot it and delete the internal low battery flag. Dispose the used batteries, as per statutory regulations. Insert the battery with plus (+) symbol facing outward Secure the battery cover.
  • Réglage de la sensibilité de détection

    Unica - Détecteur de mouvement avec interrupteur 10 A connecté – Guide de l'utilisateur de l’appareil Wiser Home

  • Remover o dispositivo do sistema

    Sistema M e Sistema D - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    Remover o dispositivo do sistema Remover o dispositivo do sistema Remover o dispositivo do sistema Pode remover o interruptor sem fios do sistema Wiser. No ecrã Inicial, toque em . Toque em Dispositivos Interruptor sem fios conectável duplo Eliminar (A). Ao remover o dispositivo, este será reposto nas predefinições de fábrica. Se o dispositivo permanecer no sistema, reponha-o manualmente. Consulte Repor o dispositivo.
  • Gerätesteuerung

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    . Tippen Sie im Startbildschirm auf die Registerkarte Kontrolle . Sie können auch die Registerkarte Kontrolle als Standard-Startbildschirm festlegen. Gehen Sie dazu auf Startbildschirm und aktivieren Sie den Schalter Mit dem Bildschirm Kontrolle starten. A Schnelle Steuerung eines Geräts (z. B. Ein
Page 870 of 989