About the device
The device can be configured through the Wiser Home app.
Advantage of using a Wireless switch:
-
Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones.
-
Easy to install on the wall: no wiring required.
-
Easy to control in places where you wouldn't normally be able to install switches.
Features of a Wireless switch:
-
Using the app, you can add various Actions (such as lighting/shutter control) to the Wireless switch.
-
Using the app, you can add a Moment to the Wireless switch (such as Movie Night MOMENT/Good Night MOMENT).
-
Low battery notification in the app.
-
This device user guide shows pairing, configuration and other features of connected Wireless switch 2-gang. The same applies for connected Wireless switch 1-gang.
-
Construction materials may cause interference which affect Hub-to-device and device-to-device distances. In the open air, there is no interference, so the distance can be much longer.
-
Wireless switch can be used as part of Quick Home Connect room control solution.