Anti-Tripping Management
-
When a device is managed by the Anti-Tripping management, the Schedules, Moments and Automations for that device are not executed.
-
This feature is available only in France and Germany.
Supported devices:
-
Power Micromodule (Water Heater)
-
EV Socket
-
Smart Plug
-
Smart Sockets
Pre-requisite:
-
Configure one of your PowerTag as Grid. Refer to Pairing main PowerTag.
-
Set the Contract limit.
A default contract limit is automatically set when pairing the main PowerTag as Grid. You can change the contract limit later if the Grid value set during the PowerTag installation does not match the tariff, refer to Setting - Peak/Off peak rate. -
Pair the supported devices. Refer to Pairing the device (based on what devices you have installed) - Power Micromodule, EV socket, Smart Plug, Smart Socket.
Enabling Anti-Tripping Management
Once the prerequisites are completed, user gets notified that this feature is available. The Anti-Tripping screen appears on the Home page.
Disabling Anti-Tripping Management
The Anti-Tripping Management feature for the supported devices can be deactivated at any time.
-
On the Home page, tap .
Tap the toggle switch (A) for the devices you want to disable.
If the device is currently in use, a notification will prompt you that deactivating this feature may cause your power to trip. -
Tap Continue to disable.
Activation status
On the Home page and control
panel page of the devices, (A) denotes the Anti-Tripping management status.
-
The devices will typically be off for upto 10 minutes. It will restart automatically when power is available.
-
If you wish to turn on the device in Home page or control panel page, a Caution window is prompted that the device is being actively managed. Read the information and tap Go to settings and disable the toggle switch to remove the device from the Anti-Tripping Management.
Live status
When the Anti-tripping feature is active for any device, the load shedding (A) is shown in the Live tab.
Troubleshooting
Error |
Possible cause |
Solution |
|
|
Restart your Hub. |