Device presetting
You can choose one preset configuration:
| Preset | Configuration | Control type / Set point range | Cycle time* (min) |
| P1 | Heat Pump/Oil Boiler (Room sensor) | Room
Control 4°C ~ 30°C |
20 |
| P2 | Hydronic Radiator/Gas Boiler (Room sensor) | 10 | |
| P3 | Hydronic Underfloor (Room sensor) | 10 | |
| P4 | Electrical Radiator (Room sensor) | 10 | |
| P5 | Electrical
Underfloor (Room sensor - without floor limit sensor) |
10 | |
| P6 | Electrical Underfloor (Room sensor - with floor limit sensor) |
10 |
*Cycle time: This setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle time may be more appropriate for slow heating surfaces, such as a concrete floor. A short cycle time is more appropriate for faster heating surfaces, such as an electric panel heater.
Initial preset configuration (by default)
When the thermostat is first powered
on or immediately after a factory reset, by default “P5” flashes on the matrix LED’s indicate Preset 5 is
selected.
Modifying the preset value
When the rotary push-button is turned clockwise, it increases the preset value by 1 and rotating rotary push-button anti-clockwise, it decreases the preset value by 1.
For example, when the rotary push-button
is turned clockwise, preset P1 becomes P2, continue rotating the rotary
push-button clockwise, and the preset changes to P3, P4...P6.
Confirming the preset
Select the preset that meets your needs by turning
the rotary push-button, and then hold the rotary push-button for >
1 s to confirm the selection.
For example, P1 is confirmed.