DUG_Micro Module Light Switch_WH-04

Editing a moment

  1. On the Home page, tap Automations .
  2. Go to Moments, locate the moment you want to edit and tap .
  3. On the Moment editor page, you can perform following changes:
    • Change the icon .

    • Rename the moment.

    • Tap each action to change the settings.

      • To remove an action, slide the action to the left and then tap (A) to delete it.

      • Tap ⊕ Add actions (B) to add new action.

  4. Tap Save to save the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?