DUG_Micro Module Light Switch_WH-07

Removing the device

  1. On the Home screen, tap .
  2. Tap Devices > Micromodule Switch > Delete (A).
    NOTE:
    • Removing the device will reset the puck. After reset, the LED turns amber indicating that the puck is ready to pair with another network.

    • If there is a problem while pairing or resetting the puck, refer to Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?