Manual sensor settings
Selecting floor sensor type
After preset, you will enter floor sensor selection menu where you can manually select the sensor type connected to the thermostat after setting the preset; this allows the thermostat to convert and display the temperature accurately.
To select the floor sensor type:
-
Once you enter the selection menu, “10” will be displayed on the thermostat dot matrix. On the device turn rotary push-button clockwise and anti-clockwise to switch between the sensor types.
Following are the available sensor type:-
10 kOhm
-
12 kOhm
-
15 kOhm
-
33 kOhm
-
47 kOhm
TIP: When the rotary push-button is turned clockwise, sensor type 10 becomes 12. Continue rotating the rotary push-button clockwise, the type changes to 15, 33, and 47.
When the rotary push-button is turned anti-clockwise, sensor type 47 becomes 33. Continue rotating the rotary push-button anti-clockwise, the type changes to 15, 12, and 10. -
-
Select the sensor type which is installed and then press the rotary push-button for > 1 s to confirm the selection.
The thermostat dot-matrix display the sensor type and LED flashes blue.
Setting temperature calibration
After selecting the floor sensor type, you must set the calibration value (offset value) of the sensor in order to minimize any variation in temperature measurement.
To set temperature calibration:
-
Turn the rotary push-button clockwise or anti-clockwise on the device to set the calibration value.
NOTE: The temperature calibration ranges from -9°C to +9°C and can be adjusted in 0.5°C increments. -
Set the calibration value, press the rotary push-button for > 1 s to confirm the selection.
The thermostat dot-matrix display calibration value and LED flashes purple.
Setting maximum guard temperature
After
setting temperature calibration, you must set the maximum guard temperature.
It is upper limit of the floor sensor.
Minimum guard
temperature can only be set through Wiser Home app.
To set maximum guard temperature:
-
Turn the rotary push-button clockwise or anti-clockwise on the device to set the maximum limit.
NOTE: The temperature limit ranges from 11°C to 40°C. -
Set the value, press the rotary push-button for > 1 s to confirm the selection.
The thermostat dot-matrix display calibration value and LED flashes red.
-
You can also perform a factory reset to remove all settings and configure the thermostat newly. Refer resetting the device.
-
It is possible to modify or update sensor settings without resetting the thermostat with the Wiser Home app. Refer floor sensor setting.