DUG_Micro Module Dimmer_WH-03

Setting the minimum and maximum brightness level

If the dimmer is connected to an LED, the minimum and maximum brightness should be set to avoid flickering and switching off the LED.
  1. On the Home page, tap .
  2. Tap Devices > Micromodule Dimmer .
  3. Drag the slider bar to increase or decrease the Minimum Brightness and Maximum Brightness (A).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?