Example of an automation

This demonstration guides you through setting up an automation that activates heating to a set temperature of 20 °C when the room temperature drops below 18 °C.

NOTE: To ensure proper heating control, you must create two separate automations:
  • Automation 1: Boost the heating when a presence is detected in the room.

  • Automation 2: Turn off the heater when the room temperature reaches 25 °C or higher.


The room heater will not turn off automatically until you create another automation.
  1. Go to Automation > to create an automation.
  2. To add a condition, tap Add Condition > Device status change > Temperature/Humidity Sensor > Temperature.
  3. Set the temperature as 18 °C (A) and the condition as less than (B) and tap Set.
  4. Read the information and tap OK.
  5. To add an action, tap Then > Add an action > Control a device > Heating > Setpoint. Set the temperature to 20 °C (C), then tap Set.
  6. Read the information and tap OK.
  7. Enter the name of the automation.
    TIP: You can choose the cover image that represents your automation by tapping .
  8. Tap Save.
    Once the automation is saved, it is visible on the Automation tab.
    NOTE: You can enable or disable saved automations on the Automations tab by using (D).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?