System User Guide Wiser Home (France) - 15

Handling QR code Issues

Condition

Action

If you are unable to find the QR code or if your hub is Wiser HubR, which does not support QR code scanning.

Tap I can't find the correct QR code and proceed to Adding a Device.

If the QR code is incorrect, a message Incorrect QR code scanned will appear.

Tap I can't scan the QR code and choose one of the following options:

  • (E): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.

  • (F): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.