System User Guide Wiser Home (France) - 15

Setting-up No Consumption Alarm

This topic explains how to setup a No Consumption alarm for a device.
  1. On the Notifications and Alarms screen, tap Create a new alarm (A).
  2. Choose alarm type as No consumption (B).
  3. Select the device from the device list and tap Next (C).
  4. Tap icon (D) and set the duration for which the device should remain at 0 Watts before triggering the alarm. Tap the Save (E).
  5. To delete an alarm, select the device and tap Delete (F).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.