System User Guide Wiser Home (France) - 15

Climate

NOTE:

Not all Devices can be added to all Wiser Hubs. To find out if a Device can be added to your Hub, please check chapter Device compatibility list

Wiser Radiator Thermostat

CCTFR6100
CCTFR6101

Provides individual temperature control for radiators.

Instruction Sheet (PDF)

Device User Guide

Wiser Room Thermostat with display

CCTFR6400
CCTFR6401

Wireless, battery-powered, colored touch-button display to set the room temperature.

Instruction Sheet (PDF)

Device User Guide

Wiser 16 A Relay for Temperature Control

CCTFR6700

Control electrical heaters with On/Off commands (Relay output) or Fil Pilote commands.

Instruction Sheet (PDF)

Device User Guide

Wiser Underfloor Heating Connection Strip

CCTFR6600
CCTFR6610
CCTFR6620

Control thermal actuator valve heads to regulate the flow of hot water in the underfloor pipes.

Instruction Sheet (PDF)

Device User Guide

Wiser Boiler Relay

CCTFR6001

Allows control of a domestic boiler in water based central heating applications.

Instruction Sheet

Device User Guide

Connected Thermostat 2 A

S5x0619

Used for water-based heating and cooling applications, such as water-based underfloor heating and radiator heating.

Instruction Sheet

Device User Guide

Wiser Micromodule for Fil Pilote Radiators

THG_CCTFR6710

The Wiser Micromodule for Fil Pilote Radiators is intended for controlling FIP compatible electric heaters.

Instruction Sheet (PDF)

Device User Guide

Wiser Temperature/Humidity Sensor

CCT593012

Measures temperature and humidity

Instruction Sheet (PDF)

Device User Guide

Connected Thermostat 2 A

S920502

S940502

Used for water-based heating and cooling applications, such as water-based underfloor heating and radiator heating.

Instruction Sheet

Device User Guide

Third party devices

Devices that are compatible with a Wiser system, but not provided by Schneider Electric.

Airzone Plenum

Zoning system for HVAC (heating, ventilation, and air conditioning) used in buildings that regulates the indoor temperature.

Device User Guide

Aidoo Pro Air conditioner

It is a solution that lets you control individual air conditioner through the Wiser Home app. An Aidoo Pro Air conditioner is wired to the AC and connects to the Wiser Home app via Wi-Fi®.

Device User Guide

Aidoo Pro Heat Pump

It is a solution that lets you control the heat pump through the Wiser Home app. An Aidoo Pro Heat Pump is wired to the heat pump and connects to the Wiser Home app via Wi-Fi®.

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.