System User Guide Wiser Home (France) - 15

Live

Provides the live data of the energy production and consumption within your home. It helps you monitor energy sources and understand how much power is being used by various devices.
From the tab, tap Live.

A

Displays live data on the power generated by various sources, such as solar panels.

IMPORTANT: The live power flow view is intended for quick, real-time checks and not designed to remain open for extended periods. If it stays open for more than a few consecutive minutes, the system will stop updating live data automatically.

B

Lists major categories of devices and their real-time power usage in kilowatts (kW), helping you track energy consumption of each device.

NOTE: If more than four devices are tracked, the energy consumption of the remaining devices will be shown as other loads, representing the total energy consumption of all these devices.

C

A graph represents energy production throughout the day. Peaks in the graph indicate higher output during specific hours.

D

Displays the total energy generated by each energy source for the current day, measured in kilowatt-hours (kWh).

NOTE: If there are no source available such as solar, battery etc., A, C, and D will not be available.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.