DUG_Micro Module Dimmer_WH-07

Resetting the Device in Quick Home Connect

It is necessary to reset the devices in the following scenarios:
  • Unpair the device in Quick Home Connect:

  • Refer to

        When reset is done successfully. The Wireless switch and device returns to factory default.

        • Integrating into Wiser System

          • If you wish to integrate the devices into Wiser System, reset all the devices in Quick Home Connect and refer to pairing the device with Wiser Hub/Gateway.

        QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

        Was this helpful?